Tool/software:
TPS65100 custom EVK not working
Below is the circuit


Voltage set at VIN = 3.3v
Current Drawn at no load 0.030 A
Wave form at SW pin =3.3V (FLAT DC)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi DGR,
Do you have the start-up waveform of VIN, SW and VOUT1 with the oscilloscope?
BR
Patrick
During startup the SW pin Goes to 3.3V Without generating any waveform and VIN Remains stable at 3.3 and Vout1 at 3.3v Respectively.
Could you suggest me how to start the TPS65100 with only VOUT1 Enabled so we can check the main switcher.
Hi DGR,
OK, could you please also monitor REF and COMP voltage during the start-up? And have you connected EN and ENR to VIN?
BR
Patrick

Image Showing Waveform at the SW pin
Image Showing AC Component at the Vout 1 (Main Boost Convertor)
Image Showing DC Component at VOUT 1
Hi Patrick,
I can see that the switching is taking place at the SW pin. Please check the waveform as I am not getting output from the Vout 2,Vout 3 Pins and Vout 4 Is only producing -2.2v
VOUT1= 9.632
VCOMIN = 3.363
VOUT2= -2.23V
VOUT3= 1.02mV
VOUT4= 1.74V
Hi DGR,
Have you confirmed the SW waveform is correct? If the VOUT1=9.6V, the SW voltage should not be that small.
BR
Patrick
So I have changed couple of things to make this board work.
C2-/mode was shorted to ground so I have removed it from there and connected the cap directly to pin 15 and 14
Now I am getting the following readings-
REF =1.65V
Vout 1= 9.62V (connected 35 Ohms Resistance as load)
Vout 2= -3.54V
Vout 3= 460 mV
VCOMIN = 1.72 V
Wave for at SW pin is attached

Hi DGR,
Ok, so could you please upload your latest schematic? Thanks
BR
Patrick
Hi DGR,
Have you tried with an inductor with higher current capability? The CDRH4D28NP-270NC seems only has 0.58A current rating.
BR
Patrick
Hi Patrick,
Yes, I am using an 4.7uH 3A 20% 39mOhm Shielded Wirewound Power Inductor.
jlcpcb.com/.../C48496
Hi DGR,
If the 35ohm resistor is removed, then what is the voltage of VOUT1?
BR
Patrick
Hi DGR,
In your previous reply, Vou1=9.62V but VCOMIN is only 1.72V? Have you confirmed the R6 and R7 are both 511kohm?
Vout 1= 9.62V (connected 35 Ohms Resistance as load)
Vout 2= -3.54V
Vout 3= 460 mV
VCOMIN = 1.72 V
BR
Patrick
Hi DGR,
Yes, this is strange, have you tried changing the IC with another pcs? Will every IC have the same behavior?
OK, could you please capture the start-up waveform of VOUT1, VREF, SW and put them in one oscilloscope screenshot? You can use 3 probes to do this.
Hi DGR,
Thanks, and could you please capture the waveforms with a longer time, like 1ms/div. I want to see when the IC stops working after power up.
BR
Patrick
Hi DGR,
So could you please also capture the waveform of the Locked up board and with longer than 1ms/div? Thanks
BR
Patrick
Hi Patrick,
Good News, I have populated a fresh board with fresh components and I can tell that I am getting better results now.
Input voltage 3.3V
Current at Input side =0.043mA
VOUT1=9.946V
VOUT2= -4.78v
VOUT3= 20.2V
VCOM= 4.986v
VCOMIN= 4.85V
REF= 1.21V
These measurements are done without any load.
I believe we can build fresh batches just to be sure that we have reached our goal.
Next thing - To test these output under load.
And Is there any way of getting 5-6 samples of TPS65100 because the TI portal is showing out of stock?
Hi DGR,
Are you available to ARROW? You can find samples there.
BR
Patrick