This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck-Boost High-side switch RC Snubber

Hello,

 

I have just read ("Minimizing Ringing at the Switch Node of a Boost Converter - SLVA255), and was wondering do Buck-Boost converters need RC snubbers across the switch node as well as boost converts?

And if so would you work the values out in the same fashion as for the boost converter?

Would the R and C be placed in parallel with the switch?

 

Regards

Michael Dalton

  • Typically, a snubber is not needed for a buck, boost, or buck-boost.  Good layout and proper component selection should result in a design that does not require a snubber.  The vast majority of Texas Instruments power designs do not need snubbers.  If you do have any issues with layout or noise in your circuit that can be helped with a snubber, the circuit values can be calculated using the SLVA255 application note.  The snubbers would be placed across the FETs that connect to ground.