Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO
Tool/software:
This is in continuation to my early post "BQ27Z561: Chemistry ID generated indicated different chemistry of cell"
I have logged the relax-discharge-relax cycle from my setup with bq27z561 Fuel gauge, as advised the relax period after discharge of at least 5 hours.
I have generated the report using the GPCCHEM tool, but this time too I got a data showing different chemistry of cell.
I have a lithium-ion cell, and the report mentions best match as LiMn2O4 (Co, Ni)/carbon, 4.35V
From the report: "Best chemical ID : 374 Best chemical ID max. deviation, % : 1.39"
I have attached the report, datasheet and the data that I submitted to the GPCCHEM tool.
Is it safe to use this chemistry ID and program it in the FG?
If not, can you please have a look at the report file generated and tell me which chemistry ID will be best for my cell?
ToGenerateChemistryID-report.zip
0474.C3 A&S Power Lipo 533442 3.8V 950mAh (119-1.0)中英文版(NT1713C+NTC+金手指)231011.pdf