Tool/software:
Hi team
We are using the above BUCK IC but in which we have two different markings
1. 37 TI 15Qx
2. 3C TI 15Qx
Please let us know whether both are same IC's.
If yes what is the difference between 3C and 37.
Because currently we are facing an issue in BUCK output current.
1. In 37 TI 15Qx output of LED current correctly matches with the VADJ
For ex: LED current is 840mA , of VIADJ 0.937V
2. Where us the IC with 3C TI 15QX the LED current is not accurate
Ex: LED current is 700mA with same VIADJ of 0.937V
So we are trying to Debug the issue.
Currently I required your support on this.
Thanks & Regards
Divakar B