Tool/software:
Hi,
- I'm using 4 Bq79656 EVM. for cell voltage and temperature monitoring. (without master (BQ79600)).
I am perfectly getting the voltage data from it, but for the temperature measurement, I enabled the TSREF but getting 0 value. (I checked with the multimeter as well it is coming 0V in TSREF pin)
please help me in this.
- And please let me know the steps need to be followed to collect temperature data from GPIO pins (Hardware and software side as well).
- What is the multiplier need to be used for ADC conversion as well.
Thanks, and Regards
Abhaya Raj Mishra