I am using the TPS65053 in a design but have no need for DCDC1. How should the L1 and FB_DCDC1 pins be connected if DCDC1 is not used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using the TPS65053 in a design but have no need for DCDC1. How should the L1 and FB_DCDC1 pins be connected if DCDC1 is not used?
Note, VINDCDC1/2 must be connected to to the same potential as VCC.
If a DCDC converter is not used, the enable pin, EN_DCDC#, must be connected to ground; the inductor can be omitted and the pin, L#, should be floated. FB_DCDC# should be connected to ground as well.
Thanks, Daniel!
Aaron, let us know if you have any questions we can help with.