This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello
A quick Q.
Can the Sense Terminal of TPS3808E exceed the Vdd; for example
if the Vdd is say 3.3 V; can the Sense terminal withstand 5V?
BR
Varun
Hi Varun,
Thanks for your question!
Sense pin and VDD pin can be connected to different supply sources. Please make sure the VDD and Vsense pin voltages are not exceeding the recommended operating conditions, which is 6V.
If you are planning to use the adjustable variant, you will need a resistor divider before connecting 5V rail to Sense terminal.
Hope this helps!
Best,
Sila