This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: Power Up Failure

Part Number: LM7480-Q1

Tool/software:

Hello,

Using common source configuration, we occasionally have power-up failure.

We assumed it's related to the charge-pump cap versus input capacitance of the Mosfets : 

the following results were obtained using 100nF charge pump cap, Q1 Ciss (8900pF Typ. and 11570pF max), Q2 (4670pF Typ. and 6230pF Max.) and CdVdT = 2x4.7nF 

  • Normal Power-Up : 

CH1 : Output Voltage, CH2 Q1 Gate-Source Voltage, CH3 Q2 Gate-Source Voltage and CH4 : Enable.

  • Power-Up Failure : 

  • When reducing the CdVdT cap to 4.7nF : We can still see some struggle to power up at the beginning.

  • When Using 470nF Charge pump Cap ( which is higher than  10x(Ciss_Total+CdVdT). with 2x4.7nF CdVdT Caps : 

470nF Charge Pump cap solved the issue, with an understandable additional delay (Delta_t of approx. 3ms)

Is there anything we missed here ? is there any risk of using 390nF/470nF ?

Thanks and Regards,

Yassine