Other Parts Discussed in Thread: UCD3138, UCC29002, UCD3138128, TIDA-00653
Tool/software:
Hello everyone
I am also interested in using the UCD3138 IC to design an isolated DC-DC boost converter with the following main characteristics:
Minimum input voltage 100 Vdc,
maximum input voltage 140 Vdc,
maximum input current 18A;
output voltage 600 Vdc,
output current 3.5 A.
Total output power 2KW.
What interests me the most is to know if the UCD3138 IC has the 'active current sharing' feature, so that I can connect multiple 2KW modules in parallel and thereby increase the output power.
Thank you very much.
Gianluca"