This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AE: Suitable for ADL-N platform?

Part Number: TPS65994AE
Other Parts Discussed in Thread: TPS65991, , TPS65994

Tool/software:

Hi,

we're developing an industrial PC based on the Intel ADL-N platform and need to implement dual USB-C ports with DP alternate mode. The Intel reference design uses a TPS65991 to provide a single USB-C port, so we need another part. 

Can you please confirm whether TPS65994AE is the correct revision to use with this platform, or if we need another suffix? Additionally, could you please suggest who to contact regarding access to the secure resources? We tried through Arrow, but they said that they don't have an FAE who can help with this request. We have an NDA with TI, but I'm not 100% sure if it's still active and/or whether it covers the TPS65994.

Thanks