Part Number: UCD90160
Tool/software:
Hi Team
Consult the software functions of UCD90160:
1. Can UCD90160 support flexible configuration of power-on sequence? It is controlled by external signal_A during power-on.
During the power-on process, PWR3/PWR8 are controlled by PWR2, and in turn control the power-on of the subsequent stage power supply.
signal_A: Control power on, PWR1->PWR2_>PWR3->PWR4->PWR5->PWR6->PWR7->PWR8->PWR9->PWR10
2. The power-off sequence can be controlled by different control signals to control the specific power-off sequence.
For example, Signal-A, which controls power-on, only controls some power supplies to be powered off at the same time, and controls some power supplies to be powered off in sequence at the same time.
When powering off, it can support non-power-on control signals (Signal_A) such as Signal_C for power-off sequence control.
signal_A: Control power off, PWR1
PWR2
PWR5_>PWR4->PWR3
PWR6
PWR7
signal_C: Control power off,PWR5->PWR4_>PWR3
Thanks,
Boyan