This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992: Schematic Review

Part Number: TPS22992

Tool/software:

Good Afternoon,

I have designed a circuit using three TPS22992RXPR to control 3 power rails

The use of these components was recommended by the external system designer.

VDD_SW and DVDDLO_SW will be asserted at the same time. The desired operation for the rails (voltage/current) is:

PS_VDD_SW (0.8V/16mA) and PS_DVDDLO_SW (1.8V/1.6mA) to ramp up at different rates to settle at the same time. My requirement is that it takes no less than 100us to ramp up.

DVDD_SW will then be asserted to energize DVDD_BATT_PS (3.3V/600uA/10mA). It must also take at least 100us to ramp up

I have attached the schematic and BOM. Single pin devices with J reference designators are test points. Two pin devices with J reference designators are jumpers to isolate the power supply from the rest of the circuit on the prototype board.

Please let me know if there is any clarifying information that I can provide.

Thanks

Frank

0336.PowerSupplySchematic.pdf

TITLE:                 Bill of Materials
DATE:                  08/12/2024
DESIGN:                ps_only

Ref     MANUFACTURER           MPN                     Qty   VALUE       
Des                                                                      
=====   ====================   ====================   ====   ==========  
C75     Murata                 GRM21BZ71A226ME15L        1   22uF        
C76     Murata                 GRM21BZ71A226ME15L        1   22uF        
C77     Murata                 GRM21BZ71A226ME15L        1   22uF        
C78     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C79     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C80     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C81     Murata                 GRM155Z71A105KE01D        1   1uF         
C83     Murata                 GRM155R71H681KA01D        1   680pF       
C84     Murata                 GRM155Z71A105KE01D        1   1uF         
C85     Murata                 GRM188R71A225KE15D        1   2.2uF       
C86     Murata                 GRM188R71A225KE15D        1   2.2uF       
C87     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C88     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C89     Murata                 GRM155R71H681KA01D        1   680pF       
C90     Murata Electronics     GRM1885C1H512JA01D        1   5100pF      
C91     Murata                 GRM1885C1H222JA01D        1   2200pF      
C92     Murata                 GRM155Z71A105KE01D        1   1uF         
C93     Murata                 GRM155Z71A105KE01D        1   1uF         
C94     Murata                 GRM155Z71A105KE01D        1   1uF         
C95     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C96     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C97     Murata Electronics     GRM21BR71A106MA73L        1   10uF        
C98     Murata                 GRM32ER71A476ME15L        1   47uF        
C99     Murata                 GRM32ER71A476ME15L        1   47uF        
C100    Murata                 GRM033Z71A104KE14D        1   0.1uF       
C101    Murata                 GRM033Z71A104KE14D        1   0.1uF       
C102    Murata                 GRM033Z71A104KE14D        1   0.1uF       
C103    Murata                 GRM155Z71A105KE01D        1   1uF         
C104    Murata                 GRM155Z71A105KE01D        1   1uF         
C105    Murata                 GRM155Z71A105KE01D        1   1uF         
C106    Murata                 GRM033Z71A104KE14D        1   0.1uF       
C107    Murata                 GRM033Z71A104KE14D        1   0.1uF       
C108    Murata                 GRM033Z71A104KE14D        1   0.1uF       
CR2     Littelfuse Inc         SMF6.0A                   1   ?           
CR3     Littelfuse Inc         SMF6.0A                   1   ?           
J4      Keystone Electronics   5019                      1   ?           
J5      Keystone Electronics   5019                      1   ?           
J6      Keystone Electronics   5019                      1   ?           
J7      Keystone Electronics   5019                      1   ?           
J8      Harwin                 M20-9990246               1   ?           
J9      Harwin                 M20-9990246               1   ?           
J10     Harwin                 M20-9990246               1   ?           
J12     Harwin                 M20-9990246               1   ?           
J13     Harwin                 M20-9990246               1   ?           
J14     Keystone Electronics   5019                      1   ?           
J15     Keystone Electronics   5019                      1   ?           
J20     3M                     N2510-6003-RB             1   ?           
J21     Keystone Electronics   5019                      1   ?           
J22     Keystone Electronics   5019                      1   ?           
J23     Harwin                 M20-9990346               1   ?           
J24     Keystone Electronics   5019                      1   ?           
J25     Keystone Electronics   5019                      1   ?           
J26     Keystone Electronics   5019                      1   ?           
J27     Keystone Electronics   5019                      1   ?           
J28     Harwin                 M20-9990246               1   ?           
J29     Keystone Electronics   5019                      1   ?           
J30     Harwin                 M20-9990246               1   ?           
J31     Keystone Electronics   5019                      1   ?           
J32     Harwin                 M20-9990246               1   ?           
J33     Keystone Electronics   5019                      1   ?           
J34     Keystone Electronics   5019                      1   ?           
J35     Keystone Electronics   5019                      1   ?           
J36     Harwin                 M20-9990246               1   ?           
L1      TDK                    VLCF4020T-2R2N1R7         1   2.2uH       
L2      TDK                    VLCF4020T-2R2N1R7         1   2.2uH       
L3      TDK                    VLCF4020T-2R2N1R7         1   2.2uH       
R22     Vishay                 CRCW0603750KFKEA          1   750k        
R23     Vishay                 CRCW0603249KFKEA          1   249k        
R24     Yageo                  RC0603FR-074K75L          1   4.75k       
R25     Yageo                  RC0603FR-074K75L          1   4.75k       
R26     Vishay                 CRCW060310R0FKEA          1   10          
R27     KEMET                  RC0402BR-0710KL           1   10k         
R28     KEMET                  RC0402BR-0710KL           1   10k         
R29     KEMET                  RC0402BR-0710KL           1   10k         
R30     KEMET                  RC0402BR-0710KL           1   10k         
R31     Vishay                 CRCW0603249KFKEA          1   249k        
R32     Vishay                 CRCW060356K0FKEA          1   56k         
R33     Vishay                 CRCW0603249KFKEA          1   249k        
R34     Vishay                 CRCW060356K0FKEA          1   56k         
R35     KEMET                  RC0402BR-0710KL           1   10k         
R36     KEMET                  RC0402BR-0710KL           1   10k         
R37     KEMET                  RC0402BR-0710KL           1   10k         
R38     KEMET                  RC0402BR-0710KL           1   10k         
SW1     C&K Components         KT11P2JM34LFS             1   ?           
U3      Texas Instruments      TPS2116DRLR               1   ?           
U4      Texas Instruments      TPS65023QRHARQ1           1   ?           
U5      Texas Instruments      TPS22992RXPR              1   ?           
U6      Texas Instruments      TPS22992RXPR              1   ?           
U7      Texas Instruments      TPS22992RXPR              1   ?           
TOTAL                                                   89               
=====   ====================   ====================   ====   ==========  

  • Hello Frank,

    Schematic looks fine to me.

    Small concern is PS_VDD_SW (0.8V/16mA) is exactly the minimum ON pin voltage level to turn on (VIH).

    CT pin capacitor values are different for each load switch. I hope they are chosen based on your requirement (to control the inrush current)

    Thanks

    Amrit