Tool/software:
Deat TI experts,
My customer considers BQ25172 for their new project. And they have few questions.
1. I saw that NiMH battery charger only use constant current mode for charging.
And termination condition is explaind 2 ways in the datasheet - Programmable timer expires and battery voltage exceeds the Vout_ovp threshold.
My question is, timer expiration is for safety which the battery is charged too much time. -> This is not a normal charging condition, just the function for safety. Am I right?
And in normal condition, charging is terminated if the voltage is exceeds Vout_ovp. datasheet says that Vout_ovp rising threshold is normally 1.70V (page 7)
But the cell which my customer use is charged to fully 2.8V voltage. So in this case Vout_ovp rising threshold is 3.40V. (series 2 cell)
Then I think This cell would never exceeds this 3.40V threshold. (because full charging voltage is 2.8V) -> tharging would not stop until the timer is expires.
Am I missing something? I want to know the normal condition of charging termination in this situation.
2. Datasheet says about nonrecoverable fault mode. (BAT OCP, ISET pin short, Charge timer expires)
Is there any way to reset TS pin without using external IC?
Please check these issues. Thanks.
Best regards,
Chase