Part Number: LM3710
Other Parts Discussed in Thread: LM7310,
Tool/software:
In a previous discussion relating to this part (link) it was identified that using a single 360k pullup resistor to VIN was acceptable (so without a complete potential divider) for the EN/UVLO pin. I want to make sure that this is acceptable when VIN is higher than the EN/UVLO pin's Absolute Maximum voltage, which is 6.5V. In my application VIN could be as high as 9V.