Tool/software:
I have three evm boards connected as a stack. If I wake them up with the GUI and start polling to read the cells voltage, Can I connect the evm board with the device id 0x01 to a separate processor while it is still as a member of stack? This processor will use it to read the register about cells voltage, so that only that board’s data is receives the processor via UART during the ongoing stack connection?
The processor will not do any wake-up and auto address operations, it will only read the register of a single card.