Tool/software:
I have implemented a LM2678SD-5.0/NOPB in my design, and have run into some trouble. VIN = 24VDC, VOUT = 5VDC. I need 2 to 3A of output current but when attached to a load it will only output 800mA before the output voltage starts sagging down to 3V.
C4 | CAP CER 0.01UF | Kemet | C0805C103J5RAC7210 | |
L2 | FIXED IND 27UH 5A 40 MOHM SMD | Bourns | SRR1210A-270M | |
C7, C13 | CAP ALUM 150UF 20% 35V SMD | Nichicon | EEE-FK1E151AL | |
D15 | DIODE SCHOTTKY 60V 7A TO277A | Vishay | SS10P6-M3/87A |