This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: The maxmum temperature that the BIN pin can measure ?

Part Number: BQ27220


Tool/software:

Hi 

May i check what is the maximaum temperature that the BIN pin can measure ?

in my customer's application they need to measure temperature over 100C

  • This depends on the thermistor. If they use the default Semitec 103AT, the linearization polynomial that the gauge uses shows this performance (top&bottom lines are for typical thermistor tolerances for the 103AT):

    So this is analyzed up to 110 deg.C (which is what we use as the max. temperature)