Tool/software:
Hello Team,
We are currently developing a device on which we use TPS65988.
Our configuration will be as the following:
- port A as sink and source (sink at 20V@3A, source 5V only), dual role data
- port B as source only (5V), host only
Use Case 1: The device is powered from VBUS only, port A sinks, port B sources
Use Case 2: The device is powered externally, both port A and B sources
So our device has 2 ways of powering:
- Through external 24V
- Through USB power delivery
The problem is, when the device is externally powered from 24V, the DRD mode on port A doesn't work in Host mode. I am curious if can this be happening because TPS sees the external 24V on the PP_HV pin? When we remove the 24V connection, we see the Host mode working without problems. However, this then disables the ability of device to be powered from USB.
Could you help me on this?Let me know if you need any more details. Thanks in advance!
Bahar