Tool/software:
I am looking to disable the battery charging via this switch utilized by my battery protection IC and need to use this switch because the charger attempts to supplement and unintentionally gets charged while the wireless charger system is building up power at the input.
I plan to disable one FET to prevent current from entering the battery and exit via the body diode if needed. The design is already build, so I don't have the option to create a less lossy alternative. The body diode will only be forward biased for very short periods of time < 100ms at a voltage of around 4.45V, but there may be situations where it needs to conduct around 10mA if the system is power is not correctly power pathed by the PMIC with integrated battery charger.
Can you provide the IV characteristics of the body diode along with the maximum current rating of the forward biased body diode to make sure we are within safe limits and a sufficient operating voltage.