Tool/software:
Hello,
I am using LMG1210 gate driver ICs to drive a Full H-Bridge. I'm interested in using the LMG1210 development board, but my current rating requirements are higher than what it supports. As a solution, I’m considering using two EPC9099 development boards, which utilize the same gate driver IC but support higher current ratings. Below are my operating conditions:
- Vin: 160V DC / 6A
- PWM: Complementary PWM of 5MHz frequency and 5V amplitude.
I have a few questions regarding the use of these boards:
-
The EPC9099 is a half-bridge development board that also supports buck and boost applications. Can I configure two of these boards for a Full H-Bridge setup?
-
If a Full H-Bridge configuration is possible, what settings or jumpers should I adjust? Specifically, do I need to select the buck or boost mode?
- What will be the output node?
I have attached the data sheet .Please find the attachment. Thanks
Best Regards,
Farhan