Other Parts Discussed in Thread: LM5161
Tool/software:
Team, Is this device able to implement the IBB as below condition? thanks.
Vin:48V
Vout:-15V
Iout:300mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
Yes, it should be able to support the IBB application. If there is a chance that the input may rise higher than 48V, you may also promote the LM5161, which is 100-V, 1A rated device.
Thanks,
Richard
Thanks. Yes, customer agree with 100V offer good design margin for IBB.
Is there related ref. design or design calculation tool of IBB with LM5161?
Regards
Brian
Hi Brian,
We do not have a reference design currently with the IBB. Please refer to the application note to get started:
Thanks,
Richard