Other Parts Discussed in Thread: BQ76952, , BQ77915
Tool/software:
Good Morning,
I am designing a battery management system for 6-12S Lithium-based (LiPo) battery pack which must accept a solar input. I have leveraged the reference design for the BQ25756 charge controller, but I also wish to incorporate cell balancing with secondary protection. I am targeting the BQ76952 Monitor and Protection IC to use in series with the BQ25756. The BQ25756 provides overall pack protection and does not necessarily need MCU programming via the I2C interface. So I am looking for a good secondary cell protection option with balancing to prolong pack life. I would also prefer the secondary protector, like the BQ76952, to be hardware programmable with the option to program via MCU, just like the BQ25756.
Can you provide feedback on whether you believe this is a good solution or perhaps provide a simpler alternative? If the latter, do you have any reference designs with these two IC's so I can speed up the design process?
Thank you for your guidance. I hope you have a great weekend.
Craig.