This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130: Negative output inductor buzzing

Part Number: TPS65130

Tool/software:

The design uses the TPS65130 to convert +5V input to ±15V outputs. During testing, we observed that the inductor on the -15V output emits a buzzing noise.

This noise disappears if FB5 is disconnected, the -15V output is left without a load, or if ENN is pulled low to disable the negative voltage output.

Increasing the load to 30mA did not alleviate the problem. Do you have any recommendations? Attached are the voltage and current waveforms for inductor L4.

SCI-RN88_ 07_POWER_15V_20240612.pdfSCI-RN88 _A02-240819_TPS65130_TPS7A3901.brd