This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030-Q1: Io-max criteria

Part Number: LMR14030-Q1
Other Parts Discussed in Thread: LMR14030

Tool/software:


Hello
I'm using the LMR14030 for a source design (Vo 4V).
The source will be used for supply different modules, an RF module included, the Irms in the circuit is about 1A but  the RF module can hit 2 - 2.5A.
The question is, for the design, should Io_max be 1A or 2.5A? and, what could be a suggested transient response for Io.
Best regards.
Christian