This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25983: tps25983 vin rating 1v

Part Number: TPS25983

Tool/software:

HI Sir

we need to protect a power rail ,which vin is 1v, current is 11A

tps25983 can't support the spec, did you have any sugeestion?

thanks

  • Hi Chen,

    What all protection features do the customer need. I can suggest a load switch which can work this operating condition (Vbias is needed separately). Most of the eFuses won't work as they need minimum of 2.5V as power to the device. 

    Can you please share the end application (you can DM me if not comfortable in sharing it here)

    Load switch recommendation: https://www.ti.com/product/TPS22959

    Best Regards,
    Arush