This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54425: Factors causing input current change

Guru 11160 points
Part Number: TPS54425

Tool/software:

Hello,

My customer is using TPS54425 as shown below.

- VIN = 12V

There is a difference in input current between the development board and the mass-produced board even though the output load is the same at 5 V.

Q1. Please review the above circuit design to see if there are any problems.

Q2. Can there be a difference in input current even if the output voltage and output load are the same in the same circuit?

       Please advise on what may be causing this symptom.

Thank you.

JH