Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO
Tool/software:
Under what conditions does the SOC of BQ40Z50-R1 trigger a jump to 0? At present, I have a project that has reached the production stage and found that the SOC suddenly jumped to 0. After checking, the corresponding voltage should be 50% -60% SOC. But I'm not sure why it suddenly jumped to 0. The ambient temperature is normal at 25 ℃ -30 ℃.