This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2482: Using the TPS2482 as E-Fuse - Current Limiter

Part Number: TPS2482
Other Parts Discussed in Thread: TPS1663

Tool/software:

Hello,

We're using the TPS2482 as E-Fuse current limiter for the resistive load of 5 ohm.

VIN = 28V

R_SESNSE = 9mOhm

Current Limit = 5A

Timer cap = 330nF

R3 = 499K

R4 = 10K

Output MOSFET is SUM70030 of VISHAY

While the resistive load is disconnected, the E-Fuse is turning on by asserting EN pin.

When resistive load is attached to the output of the E-Fuse, the pulse current that occurs is 5A, but pulse width is about 10ms instead of the expected 50ms.

Appreciate for any advice of how to raise the pulse current width to be 50ms