This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92682-Q1: w/o MCU

Part Number: TPS92682-Q1

Tool/software:

Hi Team,

When using the LH mode of the TPS92682-Q1, will the register configuration revert to the default or initial setting after the chip is powered down?

The customer wants to use the 92682 without an MCU, and if the register configuration is restored to the original setting after power down, they can configure the chip via SPI before they leave the factory. An MCU is not required on the end product.

Thanks.

Regards,

Ivy