This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24079: BQ24079 application for protect IC

Part Number: BQ24079
Other Parts Discussed in Thread: LM3658, BQ25170

Tool/software:

Hi Team

my customer will use below Protect IC.

FS326-DS-20_EN.pdf

However the protection IC will trigger protection when over discharge happen and it will leave the protection when the charger is higher than 2.7V~2.9V.

Can BQ24079 provide a higher voltage than 2.7V ~2.9V when the protection trigger protection? or BQ24079 direct provide Vbus when the protection happen,

below is spec:

Vin ~ 5V and 1S battery.(4.1V)

BRs

Brian