Tool/software:
We're working with the tps25730d. The datasheet indicates pins 26, 27, 36 should be tied to either ground or the LDO. But when working with the evaluation module and looking into the users guide we notice that the TPS25730EVM schematic indicates pin 36 is a fault out and pins 26 and 27 are not tied to either ground or the LDO but divided down 1/2. What is the proper functionality?