This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AD: Thunderbolt 4 Port A and Port B behavior are different

Part Number: TPS65994AD

Tool/software:

Dear TI

Our design is PC without battery and platform is Intel RPL-U + Two HBR

Port A is Thunderbolt 4 with PD-in

Port B is Thunderbolt 4 w/o PD-in

I have some questions below:

1. System in the G3 mode we plug in boot USB to port B and power up with AC adapter,system can not recognize this USB device.

    but when we plug to port A,system can identify it.

2. System in the G3 mode when we plug in Thunderbolt dock with PD-in to port A first then plug in port B any Type-C device,port B VBUS is 0V and no any CC communication.

   if plug in port B any Type-C device first then plug Thunderbolt dock with PD-in to port A,port A VBUS is 0V and no any CC communication.

Thank you.

Knight.