Tool/software:
Hi Everyone,
I am using two TPS38900603NRTERQ1 which share an NIRQ Line with a LED and a 560R Resistor pulled to a 3.3V Rail.
There should be a maximum current of 2.7mA flowing. (3.3V - 1.75V LEd)/560R (Assuming all the current flows through one IC only).
This current is allowed according to the absolute maximum ratings, but higher than the Recommended Operating Conditions.
However, all the voltages shown in the Fusion Design Software are 0.2V (x1 Setting) and 0.8V (x4 Setting) and software does not seem to work properly.
Can the slightly higher NIRQ current cause any latch ups?
VDD, ACT and Sleep are connnected to +5V directly.
Thank you.
Kind regards
Moritz