I have a question about Application note (SWCU077).
The circuit where VPLL and NVCC_SRTC are connected to the 2nd page of "TPS659108 User Guide For i.MX508" is indicated.
The voltage range of NVCC_SRTC is 1.1V to 1.3V.
But, the voltage range of VPLL is 1.1V +/- 3%.
Is it satisfactory when using it?
And, does it have an idea for filling the demand of i.MX50?
regards,
Sakuma