Tool/software:
Hi Team,
About the UCC27211 Timing Diagrams, it is known that the UCC27211 do not have a interlock function, so if the HI LI input high, the HO & LO will output together.
but the below diagrams, it is clear to understand the TDLRR parameter is the time between input and output.
1)and the Delay Matching is a little confuse here, if the HI(low)+LI(high) input together, why HO will drop first and LO will need type 2ns to rise up, why can not the LO rise up first and HO drop down after 2ns?
2)if the UCC27211 do not have a interlock function ,the HO & LO can output together, why we still need the delay matching here to prevent short circuit here?
tks for the checking here.