Tool/software:
Hi,
I come back about this previous topic.
Here a log with BQ Studio : 8A - 7A - rest 30s.xlsx
Here the corresponding Data Flash : 8814.DF post LC amended.gg.csv
The "Number of series cell" is ok (7) ; the "Voltage Divider" = 61921. And we are with R1 ; so without scale function.
As you can see, the "Average Power" is not compliant also. However, I could observe that the ratio between "Average Power" and calculated (real) power is around 430 (always).
In any case, I don't understand the link with "Voltage Divider" and "Average Power" if we have a good voltage measured.