This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751: Use of BQ devices other than those recommended in the datasheet

Part Number: TPS25751
Other Parts Discussed in Thread: BQ24160, BQ25798

Tool/software:

Dear Sirs and Madams,

We are considering incorporating USB Type-C PD.

I understand that the TPS25751 datasheet lists the part numbers of BQ devices that it can control.

Is it possible to use BQ devices other than these?

The reason is that we would like to incorporate USB Type-C PD functionality into the BQ24160 configuration we have used in the past.

Since we cann't control it with I2C master of the TPS25751, is it okay to configure it so that the BQ24160 is controlled directly from I2C master of the host controller?

Regards,

MM