Tool/software:
Hi ,
We are working on a new project with Wi-Fi capabilities, and for power, we are using the ER34615M battery (3.6V/19Ah), which is a primary battery.
We need protection circuitry to safeguard against reverse polarity and short circuits for the project. I came across the BQ2970 but am unsure if it is suitable for primary batteries, as the datasheet mentions charging and discharging features.
Could you please provide recommendations for protection circuitry suitable for this scenario? I am open to any suggestions or alternatives you might have.
Thank you!