Tool/software:
Hello,
We are seeing differences in the peak CS signal being measured across our converter units.
Some converter units show that the CS signal doesn't completely drop to zero about 500ns before start of the next switching cycle, while other show that it drops close to zero soon after OUTC or OUTD goes low.
In the converters units where the CS signal peak reaches the expected (calculated) value at any given load, the CS signal doesn't drop to zero after OUTC/OUTD signals turn off their respective primary side MOSFETs.
While in the units where the CS signal does drop close to zero, the peak value is lower than expected.
The attached waveforms show that. At 27A load, we expect the CS signal to be around 1.84V. The signal to the right side reaches that expected value, however, the CS signal stays above zero after OUTC/OUTD have gone low.
In the signal to the left side, the CS signal is seen dropping close to zero after OUTC/OUTD turn off their respective MOSFETs, however, the peak CS signal is ~32mV lower than expected value of 1.84V.
We are unable to determine why this is happening. We checked the isolation transformer's magnetizing inductance values but they look alike across all units. We have checked the output inductor values and they look alike as well. We have probed the units to check for other differences and don't see any.
We would appreciate any help in figuring out what is causing this difference.
Sincerely,
Nitish Agrawal