We are using both the UCD90120 and UCD9081. I have installed the GUI for the UCD90120 (TI-Fusion-Digital-Power-Designer-1.8.95) and the GUI for the UCD9081 (UCD9081-EVM-GUI-3.0.0.15) on the same PC runnning Windows 7 Professional. My problem is that the GUI for the UCD9081 does not work, and it reports "No EVM found". I have measured on the I2C bus and there is no activity at all. I installed the UCD9081 GUI on another older Win XP PC, and that works fine i.e. I'm able to program my UCD9081.
Any ideas?