This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895M:About the ICD state appears after the device into repeated reboot, black screen can not be triggered situation

Part Number: BQ25895M

Tool/software:

* Created: Fri Aug 23 13:49:59 CST 2024
*
* Format: Register Name  tab Character,\t  Hexadecimal register value.
* Device: bq25895M
* BQZ Container: Charger_1_00-bq25895M.bqz
*
Input Current Limit, HIZ and ILIM pin	7F
OTG Temperature thresholds, and Input Voltage DPM Offset	1F
ADC controls, OTG Frequency, ICO, DCP, and Input Detection	71
Battery Load, WDT Reset periods, OTG and Charge Enable, and MINSYS setting	3A
Fast Charge Current Limit settings and MTK Pump enable	10
Pre-charge and Termination Current Limit settings	10
Charge Voltage Regulation Limit, Battery Low Voltage and Recharge threshold	56
Termination Current Enable, STAT pin, WDT, Safety Timer, and JEITA Charge Current	CD
IR Compensation and Thermal Regulation thresholds	D3
ICO, Extended Safety Timer, BATFET control, MTK Pump Voltage, and JEITA Charge Voltage	40
OTG Regulation Voltage and Current Limit settings	93
Charger VBUS, Charging Mode, PG, USB Input, and System Voltage Regulation status	77
WDT, OTG/VBUS OVP, Thermal Shutdown, Safety Timer, and TS pin faults	00
Input Voltage DPM settings	23
Thermal Regulation Charge Status, and ADC Battery Voltage conversion	2D
ADC System Voltage conversion	2C
ADC TS pin voltage as percentage of REGN conversion	54
VBUS status, and ADC VBUS Voltage conversion	E0
ADC Charge Current conversion	00
DPM status, and Input Current Limit setting	40
Registers reset, Input Current Optimizer status, Device ID, and Temperature Profile	7A

在测试过程中,发现有 3 台设备在连续运行约 70 天内出现反复重启。捕获日志,发现BQ25895M的寄存器配置与正常状态的寄存器配置之间存在很大差异,其中IINDPM和ICD状态有问题,附带的寄存器配置如下,因此请帮助我看看是什么原因导致了这个问题!

此外,在监控过程中,适配器在正常插入时会耗尽电池电量,并且设备状态指示在充电和充满之间浮动。