This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150:Setting of VGH output

Part Number: TPS65150


Tool/software:

Hello.
The final output voltage is output at the designed value.(AVDD 9.6V, VGH 18V, VGL -5V)
The LCD sequence didn't seem to match, so I checked it with a scope.
 
It was discovered that the voltage rise of VGH was not normal.
I tried changing the cap of the DLY2 pin, but the start section is not delayed properly.
I want to eliminate the voltage range from 0 to 9V.
The schematic is as follows:




Please check.
Thanks.