Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Tool/software:
Hello TI,
Need application help with correct TCPC configuration of TPS65987D for my application: Docking station - 100W source + USB 3.2 hub. (OPN:TPS65987DDHRSHR, Otherwise all parts bought on Mouser)
USB Hub controller - USB7206C
Buck-boost controller - TPS552882RPMR
SuperSpeed mux - HD3SS3212IRKSR
So, according to my application need to configure USB-C port data role as UFP because of USB Hub and my board works as only source (max. 20V/5A/100W).
I am using both internal switches for source path, so using Power Duo Mode. Buck-boost feedback is controlled with events "Port0 Source PDO x Negotiated" where connect correct resistance to feedback network.

I found some problem with correct TCPC configuration and don't understand what is the problem. I tried two different configs below.
1. Device - TPS65987DDH, than Standard, than Upstream facing port (UFP only). In this configuration sourcing not working. Internal switches did not turn on and also PDOx didn't trigger the feedback of Buck-boost. The only thing that worked was that the USB hub controller was recognized in the computers and connected. Project file VisionV3_config1 in attachment.
2. Device - TPS65987DDH, than Standard, than Dual role port (DRP) (and I am not sure if I choose prefer data host or power source). In this configuration sourcing works! But I noticed that USB Hub had problem with connection with Dell latitude (1year old laptop). With my old HP ProBook 450 G6 sourcing and USB Hub works correctly. Project file VisionV3_config_DRP in attachment.
So, I have question what is different in these two configuration? Also, can you tell me how to setup correct configuration for my application? Also, you can try to pre-configure it for me and share with me.
I believe you can help me. Thank you.
Best regards,
Martin