Other Parts Discussed in Thread: BQ25756
Tool/software:
Hello,
We're using the BQ25756EVM with an STM32 microcontroller to communicate with the board via I2C. Additionally, we have a digital potentiometer connected to the feedback pin, controlled by the STM32, to adjust the charging voltage.
Our goal is to charge the battery with a current of 2A and set the termination current at 1.5A. The charging process initially works without issues, but the EVM never fully terminates the charging even after the current drops below the termination threshold. When the charging current decreases to around 1A, the board begins oscillating between charging terminated and taper charging (CV) modes. During this oscillation, the Stat 1 and Stat 2 LEDs alternate, and the charging process never fully completes.
Could you help us understand why this might be happening?
Regards,
Noel