Other Parts Discussed in Thread: TLC59116
Tool/software:
Hi Team,
I'm looking for a 16-channel LED driver that can output 20mA per channel.
I did the following calculations for TLC59116F and I think it will work.
Conditions;
Vcc = 5.5V, Vout = 17V, Iout = 20mA per ch
Iout^2 x Ron x Nch
= 20mA^2 x 3.75Ω x 16ch
= 24mW
Icc x Vcc
= 13mA x 5.5V
= 71.5mW
Pd_total
= 24mW + 71.5mW
= 95.5mW
θja x Pd_total
= 78℃/W x 95.5mW =7.449℃
Ta_max + θja x Pd_total
= 85℃ + 7.449℃
= 92.449℃ < 150℃(Tj_max)
1) Is my understanding above correct?
2) The Ta of this product is 85℃. In addition to the above conditions, are there any products that support up to 105℃?
Best Regards,