This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172EVM: BQ25172 evaluation module is detecting continuously fault.

Part Number: BQ25172EVM


Tool/software:

Hi,

I am experiencing an issue with the battery charger. At first, the charger worked well for about 15 charges. After that, it started detecting faults in the middle of charging and would stop. Now, it detects a fault right from the beginning and doesn't charge the batteries at all.

Battery:

1 Cell BK120AAHU Panasonic.

ISET: 120mA  

- R ISET 2.5K

TS: Fixed on 10K

VSET:47K

TMR: 16 h

- R TMR 8.2K