Other Parts Discussed in Thread: LM5116
Tool/software:
I have a high temperature issue with a LM5116 regulator. The design is for a 24V 4A power supply with an input voltage range from 30V to 70V.
The regulator works well until the ambient temperature reaches 130C, when the output reduces to 13.5V at a 4A load

The deltaT< (regulator-heat sink), is 15C.
The schematic is:
Can you think of any reason for the voltage to reduce this badly
Regards
Roger Jefferies