This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6593-Q1: Custom Program PMICs or Socket EVM for custom programming

Part Number: TPS6593-Q1


Tool/software:

Hi,

In our AM62Ax based SOM, we are making use of the PTPS65931211RWERQ1 PMICs with a change in the program to set the input voltage to 5V instead of the default 3.3V.

We are expecting MOQ for the custom programmed PMICs to be around 3k to 5k qty. So, we need to get the PMICs for the MOQ quantity or purchase the default PMICs and subsequently modifying their programming using a socket board.

Given that the BOOSTZL-TPS6594 programming kit has been discontinued, please inform us if any compatible socket boards are available that can be used to customize the PMIC programming. This would enable us to procure and utilize these boards for our application.
 
Thanks & Regards,
Rohith M Ravi