This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22996: Vbias vs. VIN

Part Number: TPS22996


Tool/software:

Under the recommended operating conditions in the datasheet it is stated that the Input voltage must be less then Vbias.

What are the consequences of having VIN > Vbias? I.e. Vbias=3.3V VIN=4V?

  • Hello Thomas,

    Keeping VBIAS<VIN can result the device not to turn on since charge pump in this device is not strong.

    In your example it can turn on but RDSon will be high. 

    you won't get the optimal RDSon as mentioned in datasheet.

    You can connect VIN to VBIAS.

    Thanks 

    Amrit