Other Parts Discussed in Thread: TIDA-00653, UCD3138FW-BIDI
Tool/software:
Dear TI Experts,
Reference project: TIDA-00653、UCD3138FW-BIDI
I would like to ask about the calculation formula for "POSITIVE_THRESHOLD" in the init_CBC function.
1. What are the references for "0.0269" and "127"?
2. Is "1.25" referring to the center value of the ADC, and is "2.5" the maximum ADC reading voltage?
3. If the maximum current value might change in the future, would I need to modify the Current_positive_setpoint and Current_negative_setpoint values?


4. Since I will be using ADC13 for the iShare function, but the original pin was occupied, I have adjusted it to use ADC06 instead. Could you please check if this configuration is correct?
Thank you.